Specific Gravity
Specific gravity is a measure of the density of a substance relative to the density of a standard (for this case, water) and is useful for identification purposes. PTFE is the heaviest among all the polymeric materials because of its fluorine structures. Different types of filler can be placed into PTFE. Some fillers can reduce the material’s specific gravity, while some maintain the same level. Since metals are also heavy, they increase the specific gravity.
Tensile Strength
Tensile strength refers to stress and strain behavior. PTFE is different than all other thermoplastics and thermosets. PTFE is inert—nothing in nature reacts with it. When compounding for epoxies or other polymeric materials, soft fillers like glass fibers for thermoplastics, are surface modified for compatibility with the polymeric matrix they are going in. Because PTFE doesn't have any reaction with any other material, PTFE becomes a filler no matter what you put into it. There is no chemical bond between the filler and the PTFE.
Virgin PTFE typically has around 4,500 to 5,500 pounds per square in (psi) tensile strength. Since there is no bonding between the fillers and PTFE and the strength only comes from the polymeric material, any filler inserted will result in a drop in the tensile strength. Similarly, the elongation of virgin PTFE will drop from approximately 450 to 500 percent down to 250 percent. The more filler you insert, the lower this percentage drops. A good performing compound, highly filled, should still have at least 1,500 psi tensile strength and around 80 to 100 percent elongation.
When mechanically testing tensile elongation, we follow the ASTM D638 test method. For PTFE, we use mini dog bone samples and a pull-rate of two inches per minute. We position those in an Instron machine and then pull them. When a break occurs, the machine stops and measures the tensile strength elongation.
In addition to those properties, we keep stress and strain curves and also measure tensile (elastic) modulus, yield point where the material starts yielding from the plastic to elastic region, and toughness in the area under the curve. In addition to those standard ASTM test methods, we also test tensile elongation on the final parts, using ring pull and other tests, depending on the customer specifications.
Durometer (Hardness)
To test hardness, we follow the standard ASTM D2240 for Shore D, using a very sharp pin to penetrate the PTFE compound. Virgin PTFE’s hardness is typically around 55 to 56 Shore D. The highest hardness material among all the PTFE compounds (highly filled metals) is around 67 to 68.
Hardness is normally calculated as soon as there is a spike in the scale. Equilibrium is measured after approximately 10 to 15 seconds at which time the hardness drops between a range of five to seven Shore D. So, if the hardness was at 64, after ten seconds it might drop to 59 or 58.
Temperature Range
Service temperature range is very subjective. There is no specific test to determine the real service temperature range for any type of polymer or plastic because, for each application, the conditions are different. For most applications, pressure, heat, speed and potentially chemicals are involved. In general, PTFE has the widest range of temperature resistance of all the polymeric materials.
Typically, virgin PTFE can be used at plus or minus 500 degrees Fahrenheit. When fillers are added, the virgin PTFE experiences little pressure, nominal speed and either a static environment or low PV (process variable) dynamic environment. The type, amount, shape and size of the filler also play important roles and can stretch the upper temperature range of virgin PTFE to 575 degrees Fahrenheit. The melt temperature of virgin PTFE is around 628 to 630 degrees. Getting too close to that melting point can cause the material to soften and lose many of its mechanical properties. However, even at 575 degrees, virgin PTFE will not only resist the heat, but also function well without losing its performance and properties.
PTFE outperforms all other thermoplastics and polymeric materials at the melting point. When other thermoplastics reach their melt temperature, they immediately turn to liquid and viscosity drops significantly. But PTFE does not melt—it gels, which means it maintains its structural integrity. PTFE has an extremely high melt viscosity. So even at melt (or gel) temperatures, the material doesn't flow.
Why is it important? There are certain applications, especially in dry running or non-lubricated environments, where you might see big spikes in the test environment or in the application. The temperature might go up to 700 degrees. PTFE will still survive at 700 degrees or beyond. While you don’t want to go too high (some degradation properties occur), PTFE can, for a short period of time, maintain some of its mechanical properties.
Article continues in Part 2. Click on the link below for Part 2.