Voice of the Machine-SensoNODE 4+

Parker Hannifin Corporation

Designed for iPad

    • 3.6 • 5 Ratings
    • Free

Screenshots

Description

Voice of the Machine™ SensoNODE is used for diagnostics and condition monitoring for predictive maintenance. The app allows users to connect to Parker’s SensoNODE™ Blue wireless sensors to gather measurements for a wide range of applications.

Voice of the Machine™ SensoNODE puts vital information and analytics in the palm of the user’s hand. It offers real-time and historic trend information collected by SensoNODE™ Blue (Bluetooth®Low Energy) wireless sensors and presents it in a way that makes sense to user’s operation, providing the analytics needed to optimize asset performance. Data can also be easily exported and shared.

Voice of the Machine™ SensoNODE alerts users to unexpected condition changes that may damage components and equipment. As levels rise above or fall below user-defined thresholds, users are alerted to these events, giving them an opportunity to address potential issues that could harm the system over time, helping to reduce unplanned downtime and increase productivity.

Voice of the Machine™ SensoNODE works with the full sensor line of Parker's SensoNODE™ Blue products - temperature, pressure, humidity, analog converter (4-20mA), vacuum, and ServiceJunior™ CONNECT sensors.

Voice of the Machine™ SensoNODE dashboards allow users to organize, name, and color code sensors into endless combinations for increased productivity. Sensor measurement information is viewable at-a-glance in a customizable interface.

Voice of the Machine™ SensoNODE calculations allow users to perform time saving, error-reducing, predetermined calculations. Delta calculations provide realtime differences between two measurements of the same type. Compensated pressure calculations help optimize equipment - e.g. pre-charge a bladder accumulator by using the readings of a pressure sensor and temperature sensor. Dew point calculations read relative humidity and temperature data to produce a calculated signal.

What’s New

Version 3.1.18

• Updated with the latest firmware revision, allowing over-the-air updates for the newest generation of SensoNODE™ Blue sensors

Ratings and Reviews

3.6 out of 5
5 Ratings

5 Ratings

Rbp xl ,

Use these frequently

Works very well needs audible alarm to accompany visual alarm.

HTZ Cactus ,

Not bad

Not a bad app, works as intended it seems

Geart game ,

Great very helpful

I'm a mechanic that work on big equipment, great to diagnose from the cab. Can start in the cab and watch the hydraulic pressure.
But the sound meter work backwards or I'm not using it right.

App Privacy

The developer, Parker Hannifin Corporation, indicated that the app’s privacy practices may include handling of data as described below. For more information, see the developer’s privacy policy.

Data Not Linked to You

The following data may be collected but it is not linked to your identity:

  • Diagnostics
  • Other Data

Privacy practices may vary, for example, based on the features you use or your age. Learn More

More By This Developer

Parker Fitting Finder
Business
PTS Mobile
Business
SMART Pro/R Service Tool
Business
Indego
Medical
PCH Connect
Utilities
Parker Device Connect
Business

You Might Also Like

Pressure Pro CirrusSense
Business
MultiGage Reader
Productivity
IQANgo
Business
PowerAssist™
Business
Safety Reports Scan App
Business
John Deere ExpertConnect
Business